Technical FAQs

Ask a Question

What is a 9001KM40 light module?

It is a true direct supply light module. There are no resistors in it to drop the voltage, so it can be used with any voltage lamp up to 120 volts. Highter voltage lamps are not recommended due to heat, the lens will melt.


CTA-ID : 13527
Was this helpful?
What can we do to improve the information ?