Technical FAQs

Ask a Question

What does CLI mean when dispalyed in the lower right corner of the Altivar 66 keypad?

CLI when displayed in the lower right corner of display indicates that the unit is operating in current limit. Current limit will limit the current if it runs above the setpoint adjusted in parameter named current limit in menu 7.11 motor parameters. It performs this adjustment by adjusting the voltage and frequency if needed and gives indication as well with yellow light and a CLI on the screen. The adjustable value will be in amps. Also, CLI is an indication that the unit is in ramp adaptation mode due to regenerative energy.


CTA-ID : 7098
Was this helpful?
What can we do to improve the information ?