Technical FAQs

Ask a Question

What are the Main Breaker mounting nuts used on a QO130M150 load center?

Use 2342702001, 2 required per device. When the Main Breaker connector nuts are loosened or removed, retighten to 75 lbs./in. torque.

CTA-ID : 2002648
Was this helpful?
What can we do to improve the information ?