Technical FAQs

Ask a Question

Can QYU breakers be used in QO load centers?

No. This is a unit-mount variation of the QOU. It is a Supplementary Protector and is not rated for branch circuit protection.


CTA-ID : 2003358
Was this helpful?
What can we do to improve the information ?