Technical FAQs

Ask a Question

What is the part number of a UL489 single pole Multi 9 that is designed in 9 mm width?

The multi 9 single pole breaker is 18 mm not 9mm , one module is 9mm but only accessories can be had in one module. The single pole breakers take up 2 modules.


CTA-ID : 2003081
Was this helpful?
What can we do to improve the information ?