Technical FAQs

Ask a Question

What are complete catalog numbers for type A roller lever arms for L100/300 limit switches?

Complete catalog number consists of 2 letters such as AC or AJ. See digest 172 page 19-21.

CTA-ID : 2002879
Was this helpful?
What can we do to improve the information ?