Technical FAQs

Ask a Question

Is a 9001KS34K1H4 a good part number or does it have too many contacts?

It is not a good part number. A maximum of 2 contacts can be mounted on a spring return selector switch.




CTA-ID : 13578
Was this helpful?
What can we do to improve the information ?