Technical FAQs

Ask a Question

What is the minimum current setting for the ATS48?

0.4 times the nominal rating for the soft starter is the minimum current value that can be set in the In ( nominal motor current ) parameter.


CTA-ID : 2003314
Was this helpful?
What can we do to improve the information ?