Technical FAQs

Ask a Question

What is the replacement for the QO48M30DFGPW1 pre-wired generator panel?

Cross Reference

Product Line:
QO Generator Panel

Obsolete panel cross reference

There is no direct replacement for the PRE-WIRED panel. Consider non pre-wired generator panels QO48M30DSGP (30 ampere mains) or QO48M60DSGP (60 ampere mains). Manual Transfer Equipment Kits QO2DTIM, PK4DTIM4LA, PK4DTIM4HA and PK4DTIM4LAL are also available for field installation into current design QO convertible main load centers for back-up power applications.

CTA-ID : 2003026
Was this helpful?
What can we do to improve the information ?