Technical FAQs

Ask a Question

Are NQOB panels available in NEMA 4X encloasure?

They are available in a NEMA 4X fibreglass enclosure as a factory assembled only panel. 225A max. panels only. Must ship fully assembled.


CTA-ID : 2002572
Was this helpful?
What can we do to improve the information ?