Technical FAQs

Ask a Question

What type of operators are used in the enclosed ATV66 drives?

The standard is the 22mm line. XB2, ZB2 type operators were used until June of 2001.
Newer units use the XB5, ZB5 type 22 mm push buttons, selector switches and potentiometers.
With modification Q215 the operators would be 30mm 9001K type operators.

CTA-ID : 2003287
Was this helpful?
What can we do to improve the information ?