Technical FAQs

Ask a Question

What is the part number for the Modbus card for an Alitvar 66?

The Modbus, RTU, JBUS, Uni-Telway com board is VW3A66301U. It requires that the drive has a communication card carrier or an I/O extension card installed.

CTA-ID : 2003286
Was this helpful?
What can we do to improve the information ?