Technical FAQs

Ask a Question

What is the lug kit for an NSF150?

37486 is kit for one side of breaker, 1 conductor per phase, #4 to 3/0 AWG copper solid or stranded, #3 to 3/0 AWG aluminum stranded.


CTA-ID : 2003016
Was this helpful?
What can we do to improve the information ?