Technical FAQs

Ask a Question

What is the replacement interior deadfront trim for a QON442LS400 load center interior?<br />

The interior deadfront trim will consist of two separate parts. Use 8011063001 for the Main Lugs end deadfront trim. Use NQODRPL42L4 for the Branch Breaker deadront trim. For deadfront trim mounting screws use 8002506701 (6 required. Included with the NQODRPL42L4, not included with the 8011063001).

CTA-ID : 2003012
Was this helpful?
What can we do to improve the information ?