Technical FAQs

Ask a Question

What is the replacement interior deadfront trim for a QON12LS400 load center interior?<br />

The interior deadfront trim will consist of two separate parts. Use 8011063001 for the Main Lugs end deadfront trim. Use NQODRPL30L4 for the Branch Breaker deadront trim. The NQODRPL30L4 is actually a 30 circuit deadfront trim. A maximum of twelve of the 30 branch circuit twistouts should be removed for use on the twelve circuit panel. For deadfront trim mounting screws use 8002506701 (6 required).

CTA-ID : 2003009
Was this helpful?
What can we do to improve the information ?