Technical FAQs

Ask a Question

Is there a lug kit for the bus bar on the Altstart ATS46?

Issue: Is there a lug kit for the bus bar on the Altstart ATS46?
 
Product Line: ATS46
 
Environment: All
 
Cause: N/A
 
Resolution: No. Lugs should be selected to fit 0.55 inch or 14 mm holes based on the wire sizes used.
Lugs are not included with the soft starters.


 
Was this helpful?
What can we do to improve the information ?