Technical FAQs

Ask a Question

What is the replacement interior deadfront trim for a QON42MS300 load center interior?

Issue:
Deadfront for load center

Product Line:
Load Centers

Environment:
QO

Cause:
Replacement parts

Resolution:
The interior deadfront trim consists of two separate parts. The  8011632478 Main Breaker deadfront is unfortunately no longer available since 2015. Use NQODRPL42L4 for the Branch Breaker deadront trim. For deadfront trim mounting screws use 8002506701 (6 required, but are included in the trim part numbers).


CTA-ID : 2003002
Was this helpful?
What can we do to improve the information ?