Technical FAQs

Ask a Question

What is the replacement interior deadfront trim for a QON442MS300 load center interior?

Issue:
Old design repair parts

Product Line:
QO Load Centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The interior deadfront trim will consist of two separate parts. Use 8011632478 for the Main Breaker deadfront trim and use NQODRPL42L4 for the Branch Breaker deadront trim. For deadfront trim mounting screws use 8002506701 (6 required, but are included with the trim part numbers).

NOTE: The QON442MS300 is an obsolete and no longer available load center

 
Was this helpful?
What can we do to improve the information ?