Technical FAQs

Ask a Question

How do we order a 9001 KN custom legend plate?

Issue:
How do we order a 9001 KN custom legend plate?

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product selection

Resolution:
Select which style, ie, plastic or metal, size, and color of legend plate you want. Order the special marking version of the legend plate part number and specify the marking desired with the order.
9001KN299BP is the part number for a custom engraved (special marking) 1.7 inch square plastic black legend plate with white letters. All part numbers for custom engraved legends follow the same pattern, 9001KN*99**.
Be careful not to exceed the maximum number of characters and lines available. See Digest or Push Button Specifier`s Guide for maximum numbers of characters and lines that are available for each legend plate.


CTA-ID : 13564
Was this helpful?
What can we do to improve the information ?