Technical FAQs

Ask a Question

Can the main circuit breaker in the EZM3400CB be changed out to 800 amperes?

Issue:
Product design features

Product Line:
EZM metering equipment

Environment:
Main Breaker

Cause:
Application

Resolution:
No. The labeling lists the device as 400 amps maximum. For a 800amp main need to order the EZM3800CB. 


CTA-ID : 2002794
Was this helpful?
What can we do to improve the information ?