Technical FAQs

Ask a Question

What is the difference between single hole and four hole mounting of the Vario loadbreak switch?

Single hole mounts whereas the shaft is inserted through the enclosure door and a locking nut is applied to the backside to hold the operator onto the door. The four hole mounts with four screws through the black bezel and the door, and then into the switch.


CTA-ID : 2002551
Was this helpful?
What can we do to improve the information ?