Technical FAQs

Ask a Question

Can the Generator Kit, part number QCGK2, be used with the QO load centers?

Issue:
Product design feature

Product Line:
QO load centers

Environment:
Generator kit accessory

Cause:
Application

Resolution:
The generator kit QCGK2 is obsolete and no longer available. It has been replaced by QCGK3.

The QCGK2 was not designed for use in QO load centers. The QCGK2 was designed for use ONLY in QC816F..* and QC2040M...* Combination Service Entrance Devices. Likewise, the QCGK3 is not designed for use in QO load centers. It is designed for use ONLY in QC816F...* and QC2442M...* Combination Service Entrance Devices.


CTA-ID : 2002548
Was this helpful?
What can we do to improve the information ?