Technical FAQs

Ask a Question

Can the generator kit catalog number RCGK2 be used in the HOMELINE load centers?

Issue:
Product design

Product Line:
Homeline load centers

Environment:
Accessories

Cause:
Application

Resolution:
No, the RCGK2 is not designed for use in HOMELINE load centers. SEE FA100611 for the CSED catalog numbers. 


CTA-ID : 2002550
Was this helpful?
What can we do to improve the information ?