Technical FAQs

Ask a Question

Can the Altistart units be obtained in special enclosures such as NEMA 3R, 4, 4X

We provide the ATS48 in NEMA 1, 12, or 3R enclosures as a standard offerring.  
Other enclosure types may be obtained through Seneca manufacturing on a case by case basis if requested.
Also, special enclosed soft starts may be obtained through the Industrial Applications Team ( IAT )
SquareD distributors can contact Seneca and/or IAT through their field offices.
IAT website contact is  (

CTA-ID : 9866
Was this helpful?
What can we do to improve the information ?