Technical FAQs

Ask a Question

Can we get a 9001 BG201 with a normally open and normally closed contact behind each button?

No. The 9001 BG214 has this contact arrangement. It doesn`t have legend inserts on the buttons, so these will have to be added.

CTA-ID : 2003252
Was this helpful?
What can we do to improve the information ?