Technical FAQs

Ask a Question

For a SquareD/Schneider Electric Transformer Disconnect 9070SK, are there clearances for ventilation required for installing side by side or one over the other?

Clearances for 9070SK Transformer Disconnects

Product Line:
LV Transformers

Applies to 9070 Class Transformer Disconnects by SquareD/Schneider Electric

9070SK Transformer Disconnects are potentially installed in different types of locations

SquareD/Schneider makes no recommendation for the installation of the 9070SK Transformer Disconnect other than that it must be in an ambient that has a maximum of 40degC and a 24 hour average of 30degC.

CTA-ID : 2002989
Was this helpful?
What can we do to improve the information ?