Technical FAQs

Ask a Question

What are category E combination motor controls ?<br />

Refers to UL 508E Self-Protected Device for Industrial Control Equipment as shown in table 76.2 of UL508. Basically, this is an self contained unit with disconnect, branch circuit protection, motor controller and overload protection.

CTA-ID : 2002985
Was this helpful?
What can we do to improve the information ?