Technical FAQs

Ask a Question

Can the operating handle of a KA225A circuit breaker enclosure be padlocked in the ON position?

The provisions to padlock the operating handle in the ON position is not a standard feature of the enclosure. A factory special modification can be ordered that will provide the padlock ON capabilities; add suffix SPLO to the standard catalog number. For field modification, a 3/8`` maximum hole can be drilled in the Lockoff Slider to allow the handle to be locked in the ON position. Check local code regulations for acceptability. Paint metal areas exposed by drilling with PK49SP touch up paint.


CTA-ID : 2002780
Was this helpful?
What can we do to improve the information ?