Technical FAQs

Ask a Question

Can the GD4060LK lug kit for the General Duty Safety Switches be used in the Heavy Duty safety switches?

Issue:
Product Design Features

Product line:
General Duty Safety Switches

Environment:
Lug kit accessory

Cause:
Application

Resolution:
No. This kit is for use ONLY in the following 400A and 600A General Duty switches. They cannot be used on any other General Duty nor Heavy Duty Switches. 
D225N, Series E3
D325N, Series E3
D325NT, Series E3
DU325, Series E3
D226N, Series E3
D226NR, Series E1
D326N, Series E3
D326NT, Series E3
D326NR, Series E1
D326NTR, Series E1
DU326, Series E3


CTA-ID : 2002779
Was this helpful?
What can we do to improve the information ?