Technical FAQs

Ask a Question

In the ZB4 and ZB5 lines, is there an illuminated selector switch that can be used with a standard BA9 base incandesent, neon, or LED lamp?

All the ZB4 and ZB5 illuminated selector switches must be used with the protected LED light modules.

CTA-ID : 2003448
Was this helpful?
What can we do to improve the information ?