Technical FAQs

Ask a Question

What is the 2-NO, 2-NC contacts Electrical Interlock Kit for an HU362DSEI, Series F05 safety switch?

This switch is supplied with a factory installed EIK1 (1-NO, 1-NC contacts). To replace the EIK1 with 2-NO, 2-NC contacts, use EIK2.


CTA-ID : 2003233
Was this helpful?
What can we do to improve the information ?