Technical FAQs

Ask a Question

Can a HOM816L125RB load center be converted to a Main Breaker device?

Issue:
Product design features

Product line:
Homeline load centers

Environment:
Convert to main breaker

Cause:
Application

Resolution:
The answer is dependent upon the Series number of the HOM816L125RB. Series 1, Series 2 and Series 3 were considered "fixed Main Lugs" and NOT convertible to Main Breaker. The Series S01, Series S02 or Series S03 load center may be converted to a Main Breaker by using a QOM50VH (50 amp) through QOM125VH (125 amp) Main Circuit Breaker Kit. A QOM125VH would be the maximum Main Breaker allowed.




CTA-ID : 2003232
Was this helpful?
What can we do to improve the information ?