Technical FAQs

Ask a Question

What is the difference between a FH and FHP breaker?

FH breaker is an I-line panel branch breaker; the FHP is for bus mounting and has lugs on the load side only. The FHP is also provided with `P` screws to secure the base to the cover.

CTA-ID : 2003221
Was this helpful?
What can we do to improve the information ?