Technical FAQs

Ask a Question

Why is the illumination so dim for a 9001 KM12 neon lamp?

This is inherent with a neon lamp. They produce a dim peach colored light. They were used because they had a long life compaired to an incandesent lamp, 70,000 hours verses 2,000 hours. LED`s have long life, 100,000 hours, and are brighter.

CTA-ID : 13539
Was this helpful?
What can we do to improve the information ?