Technical FAQs

Ask a Question

Is an Electrical Interlock available factory installed on a 200 ampere Heavy Duty safety switch?

Yes, although Electrical Intelocks are available for field installation, they can also be provided factory installed. Add suffix EI for 1NO/1NC contacts. Add suffix EI2 for 2NO/2NC contacts.

CTA-ID : 2002763
Was this helpful?
What can we do to improve the information ?