Technical FAQs

Ask a Question

What is the part number of the one way screws (Tamperproof) for the branch connectors of a 225A NQOD panelboard?

There are a actually 2 different kinds of one-way screws. One way screws that screw into the bus bar (Part number 21593-17080) and one that goes into the connector (Part number 21593-14090).

CTA-ID : 2002752
Was this helpful?
What can we do to improve the information ?