Technical FAQs

Ask a Question

What is the number for the lug for the LAL36400 that will accept 6 - 2/0 wires?

It is the PDC6LA20. This is a power distribution connector and is not for distribution system wiring. Use for Industrial Control UL 508 applications only.

CTA-ID : 2003216
Was this helpful?
What can we do to improve the information ?