Technical FAQs

Ask a Question

What is the voltage rating of an H226N, H226NAWK, H226NDS or H226NR safety switch?<br />

This switch is rated for 240Vac or 250Vdc maximum. Horsepower ratings are applicable only to 240Vac Corner Grounded Delta systems only.

CTA-ID : 2003209
Was this helpful?
What can we do to improve the information ?