Technical FAQs

Ask a Question

What is the thread size of a 9049GF1 and GF2 floats?

The hole is tapped at 1/8-27`` for the 4`` float. This is also good for the AGG GG and HFG 9037 switches.

CTA-ID : 2003202
Was this helpful?
What can we do to improve the information ?