Technical FAQs

Ask a Question

Can you use the +24V reference for a transducer when using the device as a PI source reference on the ATV16?<br />

Issue: Can you use the +24V reference for a transducer when using the device as a PI source reference on the ATV16?<br />
 
Product Line: ATV16
 
Environment: All
 
Cause: Wiring transducer
 
Resolution: We do not recommend using the internal supply to power external devices such as transducers. This type of operation could damage the internal supply if a short develops or the ampacity may not be sufficient for external devices taking distance, etc. into consideration and need for 24v supply for internal input uses.


 
Was this helpful?
What can we do to improve the information ?