Technical FAQs

Ask a Question

The 8536 starters are designed to withstand 6 times the motor FLC, for a short time, as an inrush rating. Is there a rating like that on these lighting contactors?<br />

For lighting contactors, it is 1.5 times rated value for Tungsten Lighting and 3.0 times rated value for Ballast Lighting.

CTA-ID : 2002740
Was this helpful?
What can we do to improve the information ?