Technical FAQs

Ask a Question

Are individual connector fingers available for QO load centers?

Issue:
Old Design repair parts

Product Line:
QO Load centers

Environment
Repair parts

Cause:
Maintenance

Resolution:
No, QO load center bussing, through 225 ampere, are single piece constuction. There are no separate connector fingers used. The connector fingers are an integral part of the branch bussing structure. Older styles of load centers may have used individually mounted connector fingers, but they were not considered to be field replacement parts.

 
Was this helpful?
What can we do to improve the information ?