Technical FAQs

Ask a Question

Can the operating handle of a IK250DS circuit breaker enclosure be padlocked in the ON position?

The provisions to padlock the operating handle in the ON position is not a standard feature of the enclosure. A factory special modification can be ordered that will provide the padlock ON capabilities; add suffix SPLO to the standard catalog number. For field modification, a 3/8`` maximum hole can be drilled in the Lockoff Slider to allow the handle to be locked in the ON position. Check local code regulations for acceptability.


CTA-ID : 2002949
Was this helpful?
What can we do to improve the information ?