Technical FAQs

Ask a Question

Can the operating handle of a MA1000AWK circuit breaker enclosure be padlocked in the ON position?

The provisions to padlock the operating handle in the ON position is not a standard feature of the enclosure. A factory special modification can be ordered that will provide the padlock ON capabilities; add suffix SPLO to the standard catalog number. For field modification, a 3/8`` maximum hole can be drilled in the Lockoff Slider to allow the handle to be locked in the ON position. Check local code regulations for acceptability. Paint metal areas exposed by drilling with PK49SP touch up paint.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 2002946
Was this helpful?
What can we do to improve the information ?