Technical FAQs

Ask a Question

Are Service Disconnect circuit breakers included in a RC2M200S Meter-Main?

The Service Disconnects are not provided. They must be ordered separately and field installed. The RC2M200S will accept (1) QOM2-VH type of circuit breaker, 200 ampere maximum and (1) QO-VH type of circuit breaker, 50 ampere maximum.


CTA-ID : 2002726
Was this helpful?
What can we do to improve the information ?