Technical FAQs

Ask a Question

Is the HOM2175SB rated for use on a 50 Hz system?

Yes, it is suitable for use on 50 or 60 Hertz systems.


CTA-ID : 2003176
Was this helpful?
What can we do to improve the information ?