Technical FAQs

Ask a Question

Is the SDSB1175C rated for use on a 50 Hz system?

Yes, it is suitable for use on 50 or 60 Hertz systems.


CTA-ID : 2003177
Was this helpful?
What can we do to improve the information ?