Technical FAQs

Ask a Question

Are the neutrals in QO load centers made of Aluminum or Copper?

The Neutral Assemblies are tin plated aluminum, suitable for either copper or aluminum conductors. This information is also pertinent to HOMELINE load centers.

CTA-ID : 2003146
Was this helpful?
What can we do to improve the information ?