Technical FAQs

Ask a Question

Does the QO140M200 come with the Main Circuit Breaker factory installed?

Yes, a QOM2200VH Main Circuit Breaker is factory installed in this load center.


CTA-ID : 2003167
Was this helpful?
What can we do to improve the information ?