Technical FAQs

Ask a Question

What size wire would the H225NR neutral assembly handle?

For Series E2-E4, the neutral assembly H600SN is used in the H225NR. The H600SN wire range is (4) #1 AWG - 750 kcmil copper or (4) #2/0 AWG - 750 kcmil aluminum. The Service Ground Lug wire range is (1) #4/0 AWG - 300 kcmil aluminum or copper conductor.

CTA-ID : 2003166
Was this helpful?
What can we do to improve the information ?